3/8/2012 9:04 AM | |
Posts: 1547 Rating:
|
Hello, as I understand you right you have already configured DCOM Settings. Nevertheless I add this short description: How do you get remote access to the SIMATIC NET OPC server? To be sure, that the used OPC Client doesn't cause the problem I suggest installing the OPC Scout on the remote PC (in directory SW you will find a setup only for the OPC Scout). Some questions: Are both PC in a Domain or in a Workgroup? If yes, are both in the same? Is there a firewall installed who can block this communication? if possible disable for a test and check if DCOM ports are released. |
Follow us on