8/23/2015 8:48 PM | |
Joined: 10/13/2009 Last visit: 12/1/2023 Posts: 2 Rating:
|
Hello, I have a similar Problem: My OPC Server is running on a Beckhoff Controller. I use a Siemens TP1200 Comfort Panel. I can establish the Connection and I can browse the variables from the OPC Server. When I start the Simulation within TIA Version 13 everything runs fine. Reading / Writing variables is ok. When I download the Project in the Panel, there is no way to read or write variables. All Input / Output fields are marked with ####. Has anyone an idea where to search ? Many thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/24/2015 2:37:29 PMNew subject after splitting |
|
Follow us on