Industry Online Support
Technical Forum
4/5/2012 1:23 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Hello, mhike! So you want to change the behavior of the Loop in Alarm function, that is called from Alarm Journal? Pictures are already opening with this function and you want the faceplates to be opened too, right? I just tried to do this. I edited this script (make a backup copy!): C:\Program Files\SIEMENS\WINCC\aplib\Split Screen Manager\LoopInAl.fct the last lines are: [code] APL_OpenFaceplate(PrototypOderEinsprungsBild, Objekt, 0, NULL, NULL); return TRUE; }[/code] It works with APL faceplates only and it is not excellent, I guess, but this is where to start from. Good luck. AttachmentLoopInAlarmAndFaceplate.fct.zip (71 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on