12/4/2020 8:11 PM | |
Joined: 5/20/2012 Last visit: 7/2/2022 Posts: 3 Rating:
|
Hi, Yes you can if you use the PLC web page. |
12/11/2020 11:41 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi laimh, yes, S7-1200 can handle CVS-files, but it has to have a specific structure. Have a look to the recipe-blocks. Have a look to this application-samples: Using recipes with S7-1200Using Recipe Functions for persistent Data with SIMATIC S7-1200 and S7-1500Parameterization of Series Machines via Recipes (S7-1200 / S7-1500)There are some more application samples, that may match your requirements if this is not what you were searching for. I just used the search-function in the upper rigth of this page and searched for "S7-1200 CSV". Life can be so simple. hope this helps, regards, |
FCK WAR! |
|
Follow us on