6/30/2009 9:12 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, Did you already read this? How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated Industrial Ethernet interface of an S7-300 or S7-400 CPU or via the CP443-1 Adv? http://support.automation.siemens.com/WW/view/en/29737976 |
Best regards |
|
Follow us on