3/22/2016 12:54 PM | |
Joined: 11/8/2010 Last visit: 4/29/2024 Posts: 10 Rating: (0) |
I use same topic. My Wincc 7.2 is intalled in VMware and TIA portal is installed in other VMware. I got migration file, but when I try to open it in TIA portal VMware, I got Error message "WinCC Professional must be installed" Really??? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/23/2016 2:00:46 PMNew subject after splitting |
|
3/22/2016 1:55 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
No, that's not how it works. There are Licenses for STEP 7, Licenses for WINCC Engineering, Licenses for WinCC Runtimes and Options and so on. The software of all of the above are integrated in TIA Portal, but you choose what to install and use. The "core" would be STEP 7. With STEP 7 comes the possibility to use WinCC Basic (Basic Panels 1st and 2nd Generation) without an extra WinCC License. If you already have WinCC 7.2 you can get a combo license, which allows you to use both systems. The best tool to see which licenses you need and which is the best option for you is the Compatibility Tool: https://support.industry.siemens.com/cs/ww/en/view/64847781 |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |