11/17/2017 8:29 AM | |
Joined: 7/9/2015 Last visit: 3/21/2025 Posts: 4204 Rating:
|
Hi, did you check if Error-Bit will have state "True". This signal can only stay for one cpu cycle so you should save it. If Error gets True, also save the state - perhaps it´s different to 7000 and we will have more information. Connections in S7-1500 can be either configured in the Network view or established with the TCON, TSEND_C or TRCV_C instruction. The exception is the ISO type of connection. This has to be configured in the Network view. Please check this: https://support.industry.siemens.com/cs/ww/en/view/109486139 Regards, Towome |
|
|
This contribution was helpful to
1 thankful Users |
Follow us on