11/13/2024 8:31 PM | |
Joined: 9/29/2024 Last visit: 1/15/2025 Posts: 18 Rating:
|
Just to make it clear, I'm using PCS7 v8.2 |
11/27/2024 11:49 AM | |
Joined: 3/13/2015 Last visit: 3/11/2025 Posts: 153 Rating:
|
Hi, Do you mean that you have 2 blocks in (different) CFC's. You open the main faceplate from the block icon and open the faceplate of the second block via the first faceplate? Then you can use the JumpFaceplate1 button (on standard view) and JumpFaceplate2 button (on preview) by creating a connection in CFC between any output of the secondairy block and the respectecly input of the main block. then compile and download the OS server. This works for all APL blocks. When creating youre own blocks you can use this feature aswel, see following post forum link Best regards, Cedric |
Follow us on