9/5/2023 10:45 AM | |
Joined: 8/3/2009 Last visit: 4/24/2025 Posts: 15350 Rating:
|
Hello This should work, I used already faceplates in Popup Screens. Check that the whole element is inside the popup Screen. If the faceplate instance is only one pixel outside then it will not be shown in RT. Check also if you use any visability dynamisation. I Would also try to reset the temporary RT Data: https://support.industry.siemens.com/cs/de/en/view/109778709 Use the latest Upd2 für V18 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on