6/19/2014 9:30 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Friends One of our customer has demanded in the specifications that all Automation hardware should be able to operate from -10 to +55 Deg. C ( Although in the region where it is to be installed, the minimum temperature ever recorded is 0.1 Deg C and Maximum Recorded Temperature is 49 Deg C). We have been arguing that 0-60 Degrees is more suited for the climating conditions, however they still want us to comply with the specifications. I have gone through this FAQand also this Thread While the FAQ very nicely explains the effect of Low Air pressure on module cooling, it does not indicate anywhere the effects of low temperatures ( Below0 Deg. C ). I would request the users and experts on theforum to share there experience on this. Cheers Navnag |
There is no such thing as the last bug in a program |
|
6/19/2014 9:44 AM | |
Posts: 8946 Rating: (999) |
Use SIPLUS Hardware. Use heater and cooler in cabinet. |
Follow us on