1/13/2009 7:12 PM | |
Posts: 2661 Rating: (279)
|
Do you mean you want to display the name of the logged-in user in your message? If yes, you need to include the Message Block "User Name" in the Message List in WinCCC Alarm Control. See attachment. Regards AttachmentHow to Include User Name in a Message.pdf (70 Downloads) |
Last edited by: Phantom75 at: 1/13/2009 11:37 PM |
|
This contribution was helpful to1 thankful Users |
1/14/2009 6:06 AM | |
Posts: 261 Rating: (42) |
Thanks But my intention is to store the operator action (mouse click,Value change of an I/O fieldetc.) in Win_CC. regards ddg |
1/14/2009 3:45 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hello ddg for I/O-Field you can set the attribute "Operator Input Message" ("Properties" > "I/O Field" > "Miscellaneous") to yes. Then you get a message by changing the value. User-defined messages: http://support.automation.siemens.com/WW/view/en/24325381 or this one: http://support.automation.siemens.com/WW/view/en/25012005 Did that helps you? regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
1/29/2009 5:01 AM | |
Posts: 261 Rating: (42) |
As per your document it is showing the user name of the P.C. But I want to store the Wincc user name. regards ddg |
1/29/2009 4:58 PM | |
Posts: 2661 Rating: (279)
|
Which document? Please clarify. Thanks |
Follow us on