12/13/2014 3:10 PM | |
Posts: 211 Rating:
|
Hi all! I have to establish communication in a network with 9 nodes of S7-1200 and PC running WinCC Advanced. Each node has S7-1200 with local KP400 HMI. This local data exchange is 70bytes or 40 tags for each node. Each node has to communicate (have HMI connection) with WinCC exchanging 100 to 300 bytes (70 to 200 tags) each. (Please see drawing attached) TIA portal V13 allows me to create such network and all connections. But, Is it possible to realise? Thanks! AttachmentTopology West 00.pdf (56 Downloads) |
Follow us on