1/26/2006 6:28 PM | |
Posts: 264 Rating: (59) |
Hello Husam, I´m not sure, but perhaps you could use the Simatic Net – OLM Modules fort his application. I know that these OLM (Optical Link Modules) work with MPI for S7-300, perhaps they also run with S7-200 PPI Interface. I think the communicatino is similar to the example in this FAQ (Perhaps this could also be an alternative for you?) Easy Remote Control and Monitoring via Dedicated Line Modem This is a completly different way of communication, but also working with PC, S7-200 PPI Port, 2 Modem but viawire copper line. In my opinion you can also use an OLM e.g 6GK1502-2CB10, but as i already said, I´m not sure because I don´t know if The OLM are able to transfer the PPI Protocol.
Greetings... |