1/27/2025 1:52 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello ‘Ralebs, are you uploading the project to the OS server as a Zap file or using the "Save As" function? If you get the error message when archiving, first archive your project locally on your hard drive before transferring the project to the OS server. You can first save the entire project folder to the hard drive (using "Save As"), then compress and archive it in Windows Explorer using a zip program, and then transfer the archive to the OS server. If that doesn't help, delete your project's IM folder and try again. Information about this can be found in the FAQ: How do I delete the IM folder of my TIA Portal project? With best regards |
Follow us on