7/8/2013 9:00 PM | |
Posts: 8946 Rating: (999) |
It seems that battery is not OK any more. |
This contribution was helpful to2 thankful Users |
7/9/2013 12:41 PM | |
Posts: 26 Rating: (1) |
Seems obvious in retrospect!Thanks for pointing it out. Joe
|
7/9/2013 12:57 PM | |
Posts: 559 Rating: (87) |
Check out the ventilating Fan is working or not when you are operating on battery? May be fan is not working on battery & that's why it is heating up. |
7/9/2013 4:13 PM | |
Posts: 8946 Rating: (999) |
Use this tool for calibrating battery and monitoring CPU temperature (and some more other things): http://support.automation.siemens.com/WW/view/en/10680121 |
This contribution was helpful to1 thankful Users |
7/9/2013 6:56 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Dear ALGUDKAR RAO Its battery problem confirmed by thread starter
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
10/31/2013 3:43 AM | |
Posts: 1 Rating: (0) |
thank you for the useful advice, is it helpful for long using if I dispatch battery? |
6/2/2014 7:21 PM | |
Posts: 89 Rating: (4) |
hi, Time to buy a cooling pad,or you may clean your PG |
4/14/2015 12:25 PM | |
Joined: 4/28/2010 Last visit: 2/8/2024 Posts: 121 Rating: (0) |
Hello, I have a Field PG M3 that had been repaired from Siemens 6 months ago from a bios problem. The computer works normally, but if it has very usage it heats up and shuts down without any error. I have notice recently that the fan is not working. Tried to download the tool for calibrating and monitoring CPU temperature from the link above, but get an internal server error. Is this a temporary error or the tool has been removed from the site? Is there any way to get access to that tool to see if it is possible to detect the real problem? Thanks in advance for your attention, RC |
Last edited by: rmb_cardoso at: 4/14/2015 1:28:28 PM |
|
4/15/2015 11:09 AM | |
Posts: 46 Rating: (5) |
Hi, for me the link is working fine. I can download this file. Can you try it again, eventually there was a server failure. |
Follow us on