7/31/2015 1:02 PM | |
Joined: 10/15/2007 Last visit: 7/17/2023 Posts: 46 Rating: (3) |
Hello, let's see if I understood it correctly...you are using the following products and are trying to communicate via Simocode ES (Engineering station connected to Ethernet-CP 443-1; Port X1 or X2?) with PROFIBUS devices Simocode pro C/V connected to PROFIBUS CP443-5, or? STEP7 V5.5 SP3/SP4 (Which version do you use?) SIMOCODE ES 2007 + SP6 +
HF2
6GK7 443-1EX30-0XE0
6GK7443-5DX05-0XE0
6ES7416-2XN05-0AB0
Can you download the HWConfig to CPU416 from this engineering station connected to CP443-1? Do you get any error messages (maybe you could post a screenshot) when trying to get online to Simocode device? Cheers |
Last edited by: LostMyMind at: 7/31/2015 7:40:11 PM |
|