Industry Online Support
Technical Forum
11/16/2012 12:56 PM | |
Joined: 1/28/2009 Last visit: 1/8/2025 Posts: 6858 Rating: (1366) |
Hello , Reading the following thread would be inspiring: how can i do the positive & negitive edge in SCL?Best regards Hamid Hosseini |
This contribution was helpful to2 thankful Users |
11/16/2012 2:14 PM | |
Posts: 15 Rating: (0) |
Hello , Reading the following thread would be inspiring: how can i do the positive & negitive edge in SCL?Best regards Hamid Hosseini So the only solution is to build a customized function. But I don't understand why there aren't specific library commands for these very simple and "abused" instructions! Many thaks. |
Follow us on