Industry Online Support
Technical Forum
9/2/2011 9:00 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, Please have a look at this link: Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Which external storage locations are available on the various operator panels (WinCC flexible/ProTool) for archiving data? How are tags and alarms logged in WinCC flexible? From the manual: Note The HMI devices are suitable for the logging of relatively small volumes of data. Manage the data in several adjacent archives in a segmented circular log. The use of a large circular log has a negative effect on performance. |
Follow us on