7/19/2007 11:27 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (319)
|
Dear Toni, Your on the right path, the Scalance switches are the best way to do your job. Please don't use the OMC, those are or will be cancelled. For the Scalance you may use types from the X100 serie or types of the X200 serie. The difference is in the unmanaged (X100) and the managed (X200) switches. The X100 are switches with now further possibilitys to check anything, the X200 are switches that have a lot of possibilitys to mirror, ring-redundancy, SNMP, Email, WEB based browser... etc. For the X100 and the X200 serie there are two switches with Fiber Optic, the X104-2/X204-2 and the X106-1/X206-1, the electrical ports are in the number 4 and 6 and the fiber optical ports are in the 1 and 2. It is also possibel to use Scalance X100 Fiber Optic media converter modules to couple with more FO ports. See the manuals for the technical specifications: Industrial Ethernet Switches SCALANCE X-200 Operating Instructions SCALANCE X‑100 product line Operating Instructions Industrial Ethernet SCALANCE X-100 Media Converter Please consider that there are new typesX200 switches with Firmware versionV2.0 !! The X200 with V1 firmware could not be upgraded to V2.... |
Last edited by: Late at: 19.07.2007 23:29V1/V2 added I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
7/23/2007 10:01 AM | |
Posts: 5822 Rating: (412)
|
Dear Toni, well, if you use a Switch to connect both to the X101-1 I would have no doubt that it works. Best regards J_Bell |
Follow us on