8/6/2023 10:27 AM | |
Posts: 3 Rating:
|
Hello everybody, I have two drives ( master and slave ) working on the same time for running a belt. In emergency cases ( one motor winding burned , mechanical problem on the gear , others..) I need to start the belt with one motor only for a small period of time , witch parameter i need to change exactly? ( P1300, P640,p1520 , ...) witch other parameter??? thanks for help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/07/2023 10:28:55New subject after splitting |
|
8/7/2023 10:29 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
Closed cause question posted twice. The second thread with the subject main parameter for G130 VSD is published within the conference SINAMICS G. Jen_Moderator |
Follow us on