1/27/2009 5:43 PM | |
Posts: 5 Rating: (0) |
Hi pl tell the following parameter VALUE when we use the spindle motor 1PH7131-2PF00-0CA0 30240 & 31020 THANKS Charan Kohar |
1/27/2009 6:40 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176) |
Hi Yes, it is right. Encoder sin/cos 1 Vpp 2048 S/R See Siemens-Katalog "NC60" Kapitel 7 Asynchronmotoren. |
Karl |
|
1/28/2009 8:08 AM | |
Posts: 5 Rating: (0) |
This motor has 14 bit resolver not a 2048 encoder. so these values are not correct thanks |
1/28/2009 11:02 AM | |
Posts: 92 Rating: (7) |
dear sir, please try these enc_type --> 1 enc_resol ---> 1 or 2. i remember doing this for one drive cliq spindle with resolver. thanks, sandeep |
1/28/2009 1:45 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176) |
Sorry Here the Datasheet. AttachmentMotor.pdf (328 Downloads) |
Karl |
|
Follow us on