11/9/2023 2:51 PM | |
Joined: 8/3/2009 Last visit: 5/21/2025 Posts: 15579 Rating:
|
Hello AutoGen_3813765 so Unified can use timers in VB Script but I would not use this for this kind of action. The PLC should be used for controlling the loading and checking the timers. you can activate the sequence by loadinig a specific dataset with a timer lifetime. then it runs in PLC. after PLC detects the end of the dataset it should trigger a tag in HMI to run the systemfunktion for loading the next specified dataset (for example as parameter set element in the last one). and so on and so on... (should work theoretically but I never tried before...) or you use an option like Lince Sequence/line coordination : https://support.industry.siemens.com/cs/ww/en/view/109799475 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on