4/29/2016 2:21 PM | |
Posts: 21 Rating: (1) |
It was mentioned like this: all parameters direct reading, little endian float, no scaling required. |
5/1/2016 2:12 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello Chaya, I got idea, look to this site for perfect applications, you can simulate Modbus RTU Master and Slave on one PC, connection can be established via 2 serial ports on PC or via some USB serial adapters connected with serial cable together. You can set on Modbus Slave your destination register with needed value (50 Hz or 220V). Send request from Master application and after receive, check that frame, also you can then better understand how the Real value can be transfered/converted. http://www.simplymodbus.ca/TCP.htm Also this site can be helpful: https://en.wikipedia.org/wiki/Floating_point Give info. |
With best regards... |
|
Follow us on