Industry Online Support
Technical Forum
6/6/2009 11:21 AM | |
Posts: 11 Rating:
|
Hey all, I'm having issue's with WinCC. I'm trying to setup a test with vmware on my home pc (I'm using vmware because I don't want to actually install WinCC on my rig because I also need MySql on it). First I had a problem with installing WinCC v6.2 (only version I have) on a Windows XP SP3, but the regedit trick found here on the forums solved this for me. /tf/WW/en/Posts/18503
After WinCC got installed I upgraded it to SP3. Now that I load my test project (I'm creating standards) the "c" function "PASSLoginDialog" is unknown?? I searched the forums already a bit but didn't find a solution. The project I loaded worked fine before but that was on a Windows XP SP2 instead of SP3. It's very strange because Passlogindialog is a standard WinCC function but now I get the message that the funtion doesn't exist? Any help is welcome... |
6/6/2009 3:21 PM | |
Joined: 6/13/2006 Last visit: 2/11/2023 Posts: 341 Rating:
|
Please see the following Usefull FAQ /tf/WW/en/Posts/7125 Also look for any error logged in Diagnose folder located in programming files/siemens/wincc/diagnose reagrds, rit03 |
Last edited by: rit03 at: 6/6/2009 3:21 PM |
|
6/6/2009 3:31 PM | |
Joined: 6/13/2006 Last visit: 2/11/2023 Posts: 341 Rating:
|
For WinCC 6.2 Compatibility , please find the attched list. Sometimes It works with changes in registry file and any other tweak. But there is no gurauntee It will work in future without any problem if compatibility has not been observed. reagrds, rit03 AttachmentWinCC_V6_Kompatiblitaets_e.pdf (79 Downloads) |
Follow us on