11/4/2006 2:35 PM | |
Posts: 21 Rating: (4) |
1.Could any one tell me how to password protect my CPU 318-2, 315-2DP PLC so that no one can alter my PLC code but still can access the program. |
11/5/2006 4:58 AM | |
Posts: 21 Rating: (4) |
Thanks a lot Mr. Late I am not very conversant with S7 plc. What i wanted to do is, i have some PLC's working in my plant with cpu 315-2DP. and all the program is written in ladder logic and partialy in STL. if you could tell me how to protect the runing software from unauthorised changes. Like my technicians keep changing the ladder diagram and i want to protect the plc code so that no one can change the existing code. if you could let me know step by step procedure and send me that on yaseen3737@yahoo.com, it will great favour from you. as per your instructions i was trying to look for source files, but there are nothing there. do i need to creat one with the name you said? Kindly bear with me for my limited knowlege on S7 and pls let me know in detail what to do. Thanks and best regards. yaseen |
11/5/2006 7:19 PM | |
Posts: 433 Rating: (48) |
Hello yaseen, i think this faq is useful for you: Enabling password protection in an S7 CPU http://support.automation.siemens.com/WW/view/en/10154913 Tomcat |
11/16/2006 4:21 PM | |
Joined: 11/16/2006 Last visit: 8/5/2024 Posts: 92 Rating: (15) |
On the Internet already there are programs which remove this password protection on memory cards MMC. |
11/20/2006 5:16 PM | |
Joined: 9/27/2005 Last visit: 4/26/2024 Posts: 203 Rating: (32) |
Hallo, with STEP 7, version 5.4 there is a a new feature LOGON. http://support.automation.siemens.com/WW/view/en/18652056 Greetings Morten |
9/1/2008 1:06 PM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
Which software that removes the password from the MMC? |
Ayman Elotaify |
|
Follow us on