Industry Online Support
Technical Forum
12/21/2012 8:22 AM | |
Posts: 35 Rating: (1) |
hi i'm trying to compile and download project to the OS but i don't know which path i should select for this dialog box i use PCS7 v8.0 what can i do? thank |
12/23/2012 12:08 PM | |
Posts: 35 Rating: (1) |
yes, my ES and OS system are on a same computer |
Last edited by: -milad- at: 12/23/2012 12:09 PM |
|
12/23/2012 3:33 PM | |
Joined: 11/15/2009 Last visit: 11/5/2024 Posts: 385 Rating: (47) |
in this case is not entry needed. Regards |
12/27/2012 5:00 AM | |
Posts: 140 Rating: (7) |
HI milad, IF your ES& OS are same no need to mention any target path and no need to download the project. Once your OS compilation is done you can use as OS. |
Follow us on