4/30/2016 7:15 AM | |
Posts: 8 Rating:
|
Dear All, I have Windows 7 professional 32bit laptop with simatic manager v5.5 software.And also i have Simatic PC Adapter USB A2.With the help of that i am trying to connect with S7-300(CPU 314IFM) PLC.But it is not communicate with PLC. For that should i want to install PC Adapter USB A2 Driver software. If possible,Can Anybody send that driver software? Please tell me the instruction to connect with PLC... Thanks Kind regards Mani ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/2/2016 3:47:11 PMNew subject after splitting |
|
4/30/2016 8:32 AM | |
Joined: 5/28/2008 Last visit: 3/12/2025 Posts: 4518 Rating:
|
Hello, I can tell you where is the drivers of PC adapter to download, Here its. PC adapter firmware and drivers But actually with Step 7 V5.5 you don't need to install PC adapter driver as it's already installed. Installation of the PC Adapter USB/USB Prommer Driver with STEP7 V5.5Please check your settings: What should you watch out for when installing the USB PC adapter? Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
Follow us on