2/22/2009 10:46 AM | |
Posts: 35 Rating:
|
Dear All, We have the following configuration on site: Rack PC 847 B CP 5613 A2 card plugged in PC is connected to S5 155 H PLC through Profibus The PC was commissioned in August, 2008 and it was working fine till last week, however it has started to hang and when we reset, all the LEDs on the panel of the rack PC is ON and the PC doesnt boot up. One of the errors just before the PC hangs is the following: ------------ CP5613A2_1<- CP5613A2 (PROFIBUS) The internal CP data is written to the file C:\program files\siemens\simatic.net\CP5613_CP5614\logfiles\EXCP_CP1.bin! ADM-send-DRV-Datptr DW_Para1:0x000000ad DW_Para2:0x0000d123 ------------- The error keeps changing every time we reboot. I've attached the latest EXCP_CP1.bin file. I have updated the BIOS of the PC to the latest version, that didnt help. Then removed the card and rebooted the PC, however all the LEDs are lit for around 15-20 mins and then the PC starts and works fine. The strange part is we have exactly same redundant rack PC and CP 5613 card along with this PC and same software is running on it too and this PC never had any problems and its working fine. Can you please help me resolve the issue? Is this CP 5613 card's issue or the Rack PC itself? Thanks and regards Fazal AttachmentEXCP_CP1.zip (81 Downloads) |
5/8/2018 12:02 PM | |
Posts: 531 Rating:
|
Did you check whether the cable has current on the earth or potential between profibus and pc shielding? |
5/8/2018 4:03 PM | |
Joined: 8/3/2009 Last visit: 12/8/2023 Posts: 11813 Rating:
|
Hello I think the COMMUNICATION PROCESSOR CP 5613 PCI CARD CARD(32BIT) F. CONNECTION TO PB INCL. DP BASE SW WITH NCM PC: DP RAM INTERF. FOR DP MASTER W. PG AND FDL PROTOCOL, SINGLE LICENSE F.1 INSTALLATION, R SW, SW+ELECTR. MAN. ON CD, CLASS A, 2 LANG. (GER, EN),EXEC. UNDER MS WIN (32BIT) NT4.0 WS,SERVER; 2000PRO, SERVER, XP PRO
Is not realeased for Win7!!! https://support.industry.siemens.com/cs/ww/en/view/22611503 Perhaps its a Problem of compatibility. And its not a A2 as mentioned in the Topic Description! Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on