6/18/2008 12:39 AM | |
Posts: 2661 Rating: (279) |
Which S7-300 CPU are you using (exact order number)? Can you see the Profibus access point in the WinCC Time Synchronization editor? |
6/18/2008 12:57 AM | |
Posts: 16 Rating: (0) |
|
6/18/2008 9:03 AM | |
Posts: 1776 Rating: (95)
|
Hi, you can find additional information in the FAQ http://support.automation.siemens.com/WW/view/de/7802886 also search for "time synchronisation" in the portal and manuals |
6/18/2008 10:33 PM | |
Posts: 2661 Rating: (279) |
What is your WinCC version? Actually it does not matter because system bus communication is allowed only over Industrial Ethernet. I tried with my WinCC 6.2 SP2 and CP5511 but could not see the access point. The only way out I can think of is to set the CPU as slave over MPI and have a MPI time server in the computer acting as master. Following FAQ is worth a look: Clock synchronization: Configuration guidelines and FAQ collection PCS7 V5.x |
Follow us on