6/23/2008 5:30 PM | |
Posts: 5822 Rating:
|
Hello Jesper... check the manual: Industrial Communication with PG/PC Volume 2 - Interfaces Programming Manual and there the chapter: 2.5.9 Server service. there you see that you get a DB 1 with up to 64 kByte of data with the S7 OPC Server. This Server DB could carry up to 64 kByte to your remote PC over S7 Communication. The only problem I see, but I guess it will be none for you, is that you will get no symbols... this is not part of the PC Station parameters. Best regards J_Bell |
6/24/2008 8:59 AM | |
Posts: 279 Rating:
|
Excellent. It sounds just like what I need. I shall give it a test. Thanks again J_Bell. |
6/24/2008 10:45 AM | |
Posts: 5822 Rating:
|
You're welcome Jesper... Best regards J_Bell |
6/25/2008 11:04 AM | |
Posts: 5822 Rating:
|
Dear Jesper, yes... I guess this would be the way to choose. Best regards J_Bell |
Follow us on