10/25/2017 6:13 PM | |
Joined: 3/13/2015 Last visit: 1/17/2025 Posts: 26 Rating:
|
Yes sir, I mean it, how is I export and import the engineering station? |
10/27/2017 10:01 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello to all I would like to ask a more basically question: -> Do you need a Simatic Net Installation on the Runtime System? -->> Its because if you do not use any simatic Net Components like special CPs, Simatic Net OPC Server, any kind of Soft PLC... then you do not need a simatic Net installation and you also do not need to transfer the PC Station configuration to the Component configurator. So if you only want to run the WinCC Advnaced RT you can deactivate the use of XDB Configuration in your PC Station in TIA Portal and use the Access Point S7ONLINE. Its much more easy then otherwise. https://support.industry.siemens.com/cs/de/en/view/89852595 Bye Murof |
Last edited by: Murof at: 10/27/2017 10:02:17 AMIf this Information really helps, you could use the Rate function |
|
Follow us on