Industry Online Support
Technical Forum
6/27/2007 1:32 AM | |
Posts: 2 Rating:
|
Dear all, we want to establish a communication between a normal PC and a S400 station, with a CP 443-1, via Ethernet. For this communication we have a WinCC Flexible Advanced, and we want to connect with WinCC Runtime. On the PC side we have a Simatic Manager V5.3 + SP3. All we want to do with this project is to change the DB102 DBX0.0 in the S400 station, from the PC, and we are trying to make this for over a week with no succes. Please give us some step by step instructions on how to do this. Attached in the screenshots.zip are some screenshots of the Project that we did so far: 1) configurtation in NetPro 2) configuration in Simatic Manager 3) configuration of the WinCC communication 4) details of WinCC Runtime Looking very forward to your answer. Best regards, Andreas Attachmentscreenshots.zip (28 Downloads) |
6/27/2007 8:08 AM | |
Joined: 5/8/2006 Last visit: 1/29/2021 Posts: 1085 Rating:
|
Hi, you should check the PG/PC Interface. You need an ethernet adapter. Then you should check correctIP address of the adapter in the network settings. After that you can test the ping between the PC and PLC. Look at this FAQ: http://support.automation.siemens.com/WW/view/de/24109937 Bye |
Follow us on