3/30/2009 3:17 PM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating: (28) |
Hi, Have you the release of the CP5711? see: http://support.automation.siemens.com/WW/view/en/6GK1571-1AA00 |
Smurf |
|
4/14/2009 5:40 PM | |
Joined: 8/31/2005 Last visit: 1/20/2025 Posts: 2198 Rating: (330)
|
Please notechapter 3 of the "Released for Delivery" In my words:To use theCP5711 you need: SIMATIC NET V7.1 SP1 or STEP7 V5.4 SP5 And STEP7 V5.4 SP5 is actual not released! (status of 14. April 2009). I tested the CP5711 (in a virtual machine) withSTEP7 V5.4 SP4, SIMATIC NET V7.1 SP1 and WinCC Flex 2008 (I think with SP1), andit worked. |
|
|
4/5/2012 10:59 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Can we use thisadapter ?? It supports 32 bit.
|
4/13/2012 12:24 PM | |
Posts: 15 Rating: (1) |
i use an adapter like that one mine is from startech and it works fine only problem is that it is very easy to break it ... be carefull http://eu.startech.com/Cards-Adapters/Slot-Extension/CardBus-to-ExpressCard-Adapter~CB2EC |
4/14/2012 2:21 PM | |
Joined: 12/1/2009 Last visit: 10/27/2024 Posts: 672 Rating: (147) |
Hi everybody, I sold my old PCMCIA CP long time ago on eBay. It was doing a great job but nothing is forever. Then I baughttemporary a USB Adapter andlatertheCP5711 (USB) afterrelease. But it's hardly used, while we moved from PB to PN. Regards. |
Give us your feedback and show us your respect! |
|
4/22/2012 12:50 PM | |
Joined: 11/18/2009 Last visit: 12/12/2024 Posts: 263 Rating: (18) |
Hi Shanny I had same problem. I have bought this adapter and I use it with CP 5512. I have connected it to SIMATIC S7-400 and to SENTRON WL with COM15. http://www.delock.de/produkte/G_66214/merkmale.html It works fine. |
5/1/2012 5:43 PM | |
Posts: 947 Rating: (45) |
Hi, shanny Cp5512 discontinued. To replace them, use CP5711. For his work need only 5V, for example, from USB, unlike the adapter MPI-USB, which should be 24V and which is not all connectors MPI / Profibus. In addition, this CP, and it supports more features, including 12MBod p.s. did not notice the date of the first post. Now all the posts 2012year irrelevant, since the question was asked a few years earlier. With the "necro"post colleagues |
Last edited by: gre_m at: 5/1/2012 6:00 PM |
|
5/2/2012 10:47 AM | |
Joined: 4/11/2012 Last visit: 10/29/2024 Posts: 181 Rating: (34) |
I got a new laptop, with ExpressCard slot, and no Cardbus. However, I bought the ExpressCard to Cardbus adapter, and I connect to S300 and S400 with no problems, using the CP5512 (Siemens Simatic Net Profibus Cardbus, 6GK155-2AA00). This is the adapter I'm using, it's from a Finnish webstore, similar products should be available elsewhere also. http://www.verkkokauppa.com/fi/product/0669/cjdtc/Fuj-tech-ExpressCard-to-Cardbus-adapteri Both the Profibus connection, and the MPI connection to Siemens logic work with this adapter. |
5/3/2012 8:22 AM | |
Joined: 11/18/2009 Last visit: 12/12/2024 Posts: 263 Rating: (18) |
Similar solutions can be found. I have given him same solution as you but with other adapter. |
Follow us on