8/21/2006 9:33 AM | |
Posts: 12 Rating:
|
Hi Nemo, Thanks for the response. We used PCS7 for Server and Client installation. I mentioned WinCC versions to get some feed back from WinCC V6.0 users. Attached are the log files (zip format) including Windows events and some screen shots of the error messages. Thanks, John AttachmentServer1b.zip (121 Downloads) |
8/21/2006 10:15 AM | |
Posts: 3149 Rating:
|
Hi, in your logfiles I´ve seemlot of entries like this: 255,10.08.2006,13:51:30:406,1007001,4,,SERVER1B,SCRIPT,ExecuteError in Action @b 255,10.08.2006,14:09:36:714,1012253,4,,SERVER1B,ArchiveManager,Backup:Not enough diskspace on path \\Server1a\Archive1A\ ! 255,10.08.2006,14:09:36:714,1012252,4,,SERVER1B,ArchiveManager,Backup:invalid path ! => so check the pathes/available diskspacefor your redundancy-project and try to get rid of the ExcecuteErrors: http://support.automation.siemens.com/WW/view/en/8385493 http://support.automation.siemens.com/WW/view/en/22198106 nemo |
8/22/2006 12:53 AM | |
Posts: 12 Rating:
|
Hi Nemo, Thanks for ur response. ---------------- 255,10.08.2006,13:51:30:406,1007001,4,,SERVER1B,SCRIPT,ExecuteError in Action @b I am not sure about the meaning of this error as I could not identifythe action script @b -------------- 255,10.08.2006,14:09:36:714,1012253,4,,SERVER1B,ArchiveManager,Backup:Not enough diskspace on path \\Server1a\Archive1A\ ! 255,10.08.2006,14:09:36:714,1012252,4,,SERVER1B,ArchiveManager,Backup:invalid path ! The log files related to archive backup are correct as sometimes the backup drive reach the maximum limit or gets full. These are optical disks and mapped on to Server1a. If the Server1a crashes or shutdown, then Server1b shows a log like invalid path. The Servers work perfect all other times. There may be some other script errors as well which are basically coming from either the Power Solutions library orother WinCC add-on like ArchiveManager tool from I&S ITPS. The system crashes only when we request for a longer trend spanning two months or more. Regards, Roy |
8/22/2006 8:01 AM | |
Posts: 3149 Rating:
|
Hi, as mentioned in http://support.automation.siemens.com/WW/view/en/8385493 I´d try to catch this error in using GSC-Runtime / APDIAG: http://support.automation.siemens.com/WW/view/en/22196773 If you are displaying lots of trends for e.g. 2 months you should check as well how much resources (CPU, memory,...) on your server are available....I could imagine, that you are running in a "lack of memory/available resources". nemo |
8/22/2006 9:35 AM | |
Posts: 3149 Rating:
|
Hi, in my experience you cannot have enough RAM for any Microsoft compatible application => I would use more RAM [:D] nemo |
Follow us on