1/29/2014 11:20 AM | |
Joined: 12/13/2006 Last visit: 2/27/2024 Posts: 27 Rating: (0) |
Thanks RugbyGuy The fault is in the program and not in the I/O , but I will need communication between two PLC's and communication to the OS (Would PLC sim do it ?) Attached is a screenshoot of my project layout. |
Last edited by: CAG168 at: 1/29/2014 11:59 AMLast edited by: CAG168 at: 1/29/2014 11:21 AM |
|
1/29/2014 5:48 PM | |
Joined: 12/13/2006 Last visit: 2/27/2024 Posts: 27 Rating: (0) |
Hi RugbyGuy Thank You , I will give it a try and see how it works. I will post the result once I try it over the next days. |
This contribution was helpful to1 thankful Users |
2/9/2014 6:18 PM | |
Joined: 12/13/2006 Last visit: 2/27/2024 Posts: 27 Rating: (0) |
Hi RugbyGuy, I have try the PLCSim method, I can have more than one PLCSim Running, but PLCSim would not simulate the communication between PLCs with CP card, I think it will only simulate netwok cards which are On the CPU (e.g. PN type PLC) |
Follow us on