Industry Online Support
Technical Forum
10/21/2008 8:32 AM | |
Posts: 4 Rating: (0) |
Hi all. I'm working on a DCS PCS7 V.7 project. I need to communict with a third party device via IEC 60870 101 or 104. please help me. |
10/21/2008 11:00 AM | |
Joined: 9/27/2006 Last visit: 1/13/2025 Posts: 12325 Rating: (2697) |
Hello hami; Unless I am mistaken, there are no direct solutions in the Siemens Automation and Drives division for integrating IEC 60870 protocols. These protocols being dedicated to power and energy systems, such as substation automation, you could have a look at offerings from other Siemens divisions, such as: -Siemens Power and Industry: SIWA CIS PAS (integration of IEC 60870 to PCS 7) http://www.industry.siemens.com/ifat/EN/SOLUTIONS/AE_SIWA_CIS_PAS_WAN.HTMThere is a small brochure and a contact name (and address), not much more; if yoy are interested you will need to contact them directly. -Siemens SICAM Power Quality division: Sicam PAS: http://www.sicam.de/index_e.htmAgain you will need to contact that division (they also make Siprotec protection relays, they can be ordered with various IEC 60870 communication protocols) to get details of your integration possibilities. You could also have a look on the web on IEC 60870 gateways, such as this one: http://www.kalkitech.com/protocolsupport.htm They offer support for IEC 60870 protocols, Modbus, Profibus, eevn OPC DA. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/21/2008 11:04 AM |
|
11/17/2008 11:05 PM | |
Joined: 11/16/2008 Last visit: 10/16/2024 Posts: 4 Rating: (1) |
Hello hami, may be it is to late, but thereexists a (Siemens-) solution: SIPLUS RIC (Application) IEConS7: IEConS7 are diffrerentlibraries for S7-300 and S7-400 PLCs (CPUs)for realizing telecontrol solutions with IEC 60870-5-101and 60870-5-104 (sometimes only T101 or T104) protocol. forfurther information please follow the link: https://www.automation.siemens.com/siplus/html_76/produkte/ric/softwarebibliothek.htm or contact me (GSucher) or one of the named persons of this link: https://www.automation.siemens.com/siplus/html_76/support/service.htm |
Follow us on