1/12/2012 11:53 AM | |
Posts: 39 Rating:
|
Hello, What's your favorite choice? - modifiy the related regedit settings. - use a specific software to control usb stickcontents - use a third solution. If yes, which one? Thank you in advance Regards François |
1/13/2012 9:08 AM | |
Joined: 3/15/2008 Last visit: 11/21/2024 Posts: 106 Rating:
|
hi, I think the best option is to disable usb ports in bios. Modern machins give you that funcion nowadays. Regards |
Best regards |
|
1/16/2012 9:32 AM | |
Joined: 3/14/2008 Last visit: 3/14/2025 Posts: 2175 Rating:
|
Disable it through domain settings: You can easily create a group where USB ports are disabled. New users can be put into the group and settings automatically apply for them also, |
If I could help you, you can use the RATE button. Thank you. |
|
1/17/2012 11:41 AM | |
Joined: 4/5/2006 Last visit: 3/5/2025 Posts: 917 Rating:
|
Hi frade22, Disabling USB from bios should disable the keyboard and mouse also If you are ion domain the good solution it was Oreca said If you are in workgroup the registry modification can fail in same particular cases I faced in same problem time ago, i used free program "adl_setup"; it's not fully featured but enough for my application (nice but with no password protection from not autorized users). Search for "usb disabling..." in web browser, there are a lot of solution there even free aven cheaper with more feature regards |
1/18/2012 9:47 AM | |
Joined: 2/19/2009 Last visit: 7/9/2024 Posts: 17 Rating:
|
Hello, And hardware opcion? link |
Last edited by: Techand at: 1/18/2012 9:47 AMLast edited by: Techand at: 1/18/2012 9:47 AM |
|
Follow us on