1/29/2007 10:36 AM | |
Posts: 7 Rating: (0) |
On my Engineering Station (ES) I cannot create an OS project in the SIMATIC Manager or no OS project is displayed although it is present.
When i create PC station i can insert Indıstrial Ethernet Modul but cannotinsert WinCC aplication. and i don't have the WinccCom folder. In the existing project the OS cannot be displayed in station. Thank you very much for help. AttachmentOs_create_error.zip (301 Downloads) |
Last edited by: Abdullah at: 1/29/2007 10:38 AM |
|
1/29/2007 1:10 PM | |
Posts: 3149 Rating: (171)
|
Hi, which PCS7 version did you install? Does this happen in a new pcs7 project as well? Did you proceed acc. to this FAQ ? http://support.automation.siemens.com/WW/view/en/17581871 nemo |
1/29/2007 1:49 PM | |
Posts: 3149 Rating: (171)
|
does this happen in a new project as well? which pcs7 version are you using? |
1/29/2007 1:58 PM | |
Posts: 3149 Rating: (171)
|
Hi, could you please attach the file citamis.str at the forum? http://support.automation.siemens.com/WW/view/en/23069304 Which PCS7 version are you using? nemo |
1/29/2007 2:34 PM | |
Posts: 7 Rating: (0) |
Hallo
AttachmentCitamis.zip (293 Downloads) |
1/22/2008 8:36 PM | |
Joined: 1/22/2008 Last visit: 4/5/2024 Posts: 3 Rating: (0) |
Hi, I had the same problem and i reinstalled the PCS 7 software, but the problem continuos |
1/24/2008 8:05 PM | |
Joined: 1/22/2008 Last visit: 4/5/2024 Posts: 3 Rating: (0) |
Solution OK. Reinstalling Microsoft SQL server. |