Industry Online Support
Technical Forum
11/14/2008 12:58 PM | |
Posts: 125 Rating: (26) |
Hi, if you download with "Compile and Download Objects" then you can select the OS-Server klick on button Single Object. See Picture. |
11/14/2008 1:50 PM | |
Posts: 12 Rating: (0) |
New messages from the Front Line ;) Now I have even bigger problem.. I can't open WinCC project - see attached file.. Any ideas why ? |
11/14/2008 8:26 PM | |
Posts: 2661 Rating: (279) |
Did you try to activate the server OS on the ES? The following FAQ's may help: After reloading the OS project to the server from the ES, how do you clear the undefined error message and the abort? How can you clear the error message "Download (310:88)"? Which messages may appear in the "Download OS" dialog box? How do you use the SIMATIC shell to configure the terminal bus of a WinCC station? What should you do if the OS server project is taken online by mistake on the ES? |
Follow us on