4/2/2014 9:17 AM | |
Posts: 567 Rating: (107) |
Dear You, Siemenshasn't released PCS 7 V80 SP3. Siemens released a CFC version V8.0 SP3 which is compatible with PCS 7 V8.0 SP1. You need to update your CFC version to open your CFC charts. To find out which currentCFC version (or any other components) you could use the Compatibility Tool which you can find under the following link. http://support.automation.siemens.com/WW/view/de/2334224 There you could also see that the current CFC version is CFC V8.0 SP4 upd2. |
4/2/2014 11:20 AM | |
Posts: 4 Rating: (0) |
Hi Ralfinio, Where can I find the update for CFC SP3? I checked my current version of CFC is SP2 Upd 2.
|
4/2/2014 12:22 PM | |
Posts: 567 Rating: (107) |
Hi Yow, if it is not provided as download you have to open a service request. Link to open a service request: http://support.automation.siemens.com/WW/view/en/4000024+16605032 |
4/7/2014 9:21 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating: (40)
|
If my memory serves me correct, CFC V8.0 SP3 is also part of the download for the CPU 410 HUP which can be had herehttp://support.automation.siemens.com/WW/view/en/68627630 You can also do a free upgrade to PCS 7 V8.0 SP1 Upd1, which will take you to CFC V8.0 SP4 Upd1, which can be found here,http://support.automation.siemens.com/WW/view/en/85522559 Have a great day
|
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
This contribution was helpful to1 thankful Users |
Follow us on