8/28/2019 7:55 AM | |
Joined: 3/14/2008 Last visit: 8/30/2024 Posts: 2093 Rating:
|
Hi, Are you mounting the ISO files? if so, when asked, please remove the disk 1 from the mounted drive and mount disk 2 on the same mounted drive. So if you use letter F, disk 2 should be mounted on F as well. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
3 thankful Users |
8/28/2019 1:24 PM | |
Joined: 10/26/2011 Last visit: 8/30/2024 Posts: 762 Rating:
|
Hi, PCS 7 V9.0 is not released for Windows XP. It is desired that the installation does not work. |
Last edited by: Thunderstorm at: 08/29/2019 16:58:08SIMATIC PCS 7 - Overview |
|
Follow us on