5/14/2010 7:30 AM | |
Posts: 33 Rating: (0) |
Hi Siwarexi I am facing a peculiar problem while calibrating the siwarex i find that the gross weight goes on increasing even when no material goes in the bin so is the millivolt, i have checked the excitaion its ok,i have configured the zero as well as the span ,the load cell capacity is 22 tons and the bin mechanical weight is arount 10 tons,is there is any load cell problem if yes how can i confirm this to the user? Best Regards Zamir Splitted from Excitation voltage. |
Last edited by: O_Moderator at: 5/17/2010 10:56 AMnew subject after splitting |
|
Follow us on