4/21/2022 1:49 PM | |
Posts: 34 Rating:
|
Hello After a download of all software and warm restart of plc it is stuck in stop mode. When online the cpu operator panel says below run-stop-mres-buttons, mode selector STOP. Does not help to click RUN from TIA portal. This is the third time it happens on my lab plc. Only thing that helps is to physically push the RUN button on plc. I have a support case running with siemens without result so far. Cheers // AttachmentDiagnostics_Buffer_220421.txt (361 Downloads) |
Last edited by: tystnariluren at: 04/21/2022 13:50:10 |
|
4/22/2022 7:22 AM | |
Posts: 34 Rating:
|
Thanks for information! The important piece of info that i forgot to mention is that my plc is a 1511-1 PN. Meaning it has only a digital switch. |
Follow us on