9/2/2016 9:51 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Hi, In attachment several print screens. As you can see in print screen starter_1 it's not possible to connect to drive. I do have connection because I can ping PLC (CP-card) and go online in PLC code. AttachmentPGPC_Netpro_Starter.zip (134 Downloads) |
9/2/2016 10:08 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
Is your network card in the same network? Can you ping the device? Is there a virus scan or firewall activ? |
~(‾▿‾)~ |
|
9/2/2016 10:11 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Drive is on Profibus. CP card on IE. And yes I can ping CP. |
9/2/2016 10:21 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
No it doesn't find the specific PLC (cp-card) :s |
9/2/2016 11:11 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
As you can see in attachment, IP address and description is correct in Edit Ethernet Node and also in Accessible nodes of Simatic Manager I can find it back... AttachmentEthernetNode&AccessibleNodes.zip (77 Downloads) |
9/2/2016 11:28 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Hi, It says no further node found.. |
9/2/2016 11:35 AM | |
Joined: 5/12/2006 Last visit: 4/30/2024 Posts: 22243 Rating: (2980)
|
The SimaticManager and the Starter installed on the same System? Not on differnt Systems or Virtual machines? |
9/2/2016 1:45 PM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
I can ping it, i can go online with it... :s ... |
Last edited by: OmegaProjects at: 9/2/2016 1:49:03 PM |
|
9/2/2016 2:04 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
Then maybe a firewall or anti vir is blocking the discovery process. |
~(‾▿‾)~ |
|
Follow us on