2/26/2016 6:19 PM | |
Joined: 8/8/2014 Last visit: 6/14/2022 Posts: 52 Rating:
|
attachemnt to previous post... |
3/15/2016 5:46 PM | |
Joined: 8/8/2014 Last visit: 6/14/2022 Posts: 52 Rating:
|
in addition to the previous post - more details, I use invert logic for cooling. So when Tinside > Tsetp. PID responds, bigger error, bigger PID output, when error decrease, PID output also decreases and responds. But as soon as error = 0 , the PID output freezes , and just keeps some value not equal to 0. Seems like it goes in " hidden " inactive mode, but status output = 3 (for automatic). In this state, if I re-trigger "PID_Compact_2".sRet.i_Mode --> 0 --> 3 then PID wakes up again. I attach PID tech. obj. settings - not latest version, I also tried to remove Integral time with no effect. AttachmentPID_Compact_2_settings.pdf (379 Downloads) |
Follow us on