9/25/2013 8:18 AM | |
Joined: 1/3/2013 Last visit: 1/25/2023 Posts: 40 Rating:
|
Dear friends, I just started my experience in Siemens world and I came into some problems already, so please have patience with me I run uder Windows 7 with TIA portal V11 SP2 update 5 and I have the following setup:
Even if the setup works pretty fine...I would like to solve or have an understanding about the following issues: [schnippschnapp]
I know that this is a long thread, but I wanted to provide you with all the requied info. Looking forward for your advices! Thanks, AttachmentADC and Vacon issues.pdf (50 Downloads) |
Last edited by: O_Moderator at: 9/27/2013 11:52 AMnew subject after splitting |
|
10/4/2013 9:13 AM | |
Joined: 10/10/2005 Last visit: 11/21/2022 Posts: 1909 Rating:
|
Hello, regarding to your ADC and Vacon issue. Is the GSML file compatible with STEP 7 V11+SP2+Upd 5? Its looks as if, that this product is not still ready integrated in the project of STEP 7 (TIA Portal). I recommend to update the firmware of the S7-1200 CPU and save and compile the Vacon product in STEP 7 again. http://support.automation.siemens.com/WW/view/de/65601780 With best regards |
Follow us on