5/26/2012 7:09 PM | |
Posts: 24 Rating:
|
I'm new with the 1200 and need to limit the output of the PID compact. The output never may be less than 10%. How can I do this? greetings |
5/27/2012 1:32 PM | |
Posts: 36 Rating:
|
Hi MaanuelSeabra, You must define the limit in the settings in the PID. You give limit as you want.
|
5/27/2012 8:37 PM | |
Posts: 24 Rating:
|
OK But I set to limits Output Value haight=100 and Output Value lower limit =10and the output always varies from 0 to 100%. Should I do anything else? Thanks |
12/17/2015 2:49 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4839 Rating:
|
New question published by James Fox is split to a separate thread with the subject PID, set the LOWER limit at a positive value. Best regards |
Follow us on