6/3/2008 2:20 PM | |
Posts: 559 Rating: (87) |
Dear all, U can use symbolic PIW or PQW directly to scaling blockor unscaling blockFC105 and FC 106 in LAD itself. For What u have to do, First u give address say PIW 100 to FC105 without assigning Symbol into Symbol table. Then U save block and close it. After that u assign symbol to perticular input into symbol table, save and close it. Then U open Block In which u called FC105. Uwill find percilar PIW with Symbolic name. See the attachment. Attachmentpiw.pdf (489 Downloads) |