1/7/2021 1:43 PM | |
Joined: 9/18/2017 Last visit: 10/3/2024 Posts: 5 Rating: (0) |
Hi, I am Working On Step-5 PLC 115 U (CPU 945).Actually The Connected IPC/HMI Is Damaged .So Dont Have Original Backup .Need To Find Out Alarm Bits From Logic & Need To Attach New IPC/HMI. But I am Not Understanding The Logic /Blocks Written in PLC. which Bits/db I have To use For New hmi. They Given Alarm Management Blocks(fb20,fb21,fx48,fx41) In machine Manual. Please Find Attached File For Detail. please help me to understand Blocks & Logic. Thank You ------------------------------------------------------------------------------------------ Attachmentalarm management.zip (471 Downloads) |
Last edited by: CS Moderator at: 01/08/2021 14:49:25New subject after splitting |
|
1/23/2021 11:06 AM | |
Joined: 9/18/2017 Last visit: 10/3/2024 Posts: 5 Rating: (0) |
Thank u For Reply, Gabriele The Device Is PROVIT 2200 i.e B & R IPC 2001 Series. Actually the hard drive Failure.so there is no way to do reverse engg from HMI. When I start IPC Following condition occur on Display..plzz see attached Photos. Attachmentpics.zip (452 Downloads) |
Follow us on