4/16/2012 12:35 PM | |
Joined: 12/1/2009 Last visit: 5/2/2023 Posts: 669 Rating:
|
Hi, in order to be a profibus master, the CPUhas to have therequired interface (internal or external). https://www.automation.siemens.com/mcms/programmable-logic-controller/en/simatic-s7-controller/s7-300/cpu/compact-cpus/Documents/brochure_simatic-controller_en-43_table.pdf Yes, you can connect all your CPU's to the profibus so than they can communicate with each other. Regards. |
Give us your feedback and show us your respect! |
|
4/18/2012 11:32 AM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
My vote is for using DP/DP Coupler. Even if it is need to spend more money. Anyway: S7-300 like a Profibus slave - What master/slave communication options are available on PROFIBUS DP? DP/DP Coupler - What are the special features of input/output addressing with the DP/DP coupler?and Configuration of the I/O Data on DP/DP Coupler
Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
4/18/2012 11:40 AM | |
Joined: 8/18/2009 Last visit: 4/10/2023 Posts: 534 Rating:
|
Dear TIBI68, tell me maximum how meny slave PLC we can comunicate with one master PLC...
|
Rajkiran Patil |
|
4/18/2012 11:52 AM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
The max. slave are limited to 32 nodes without to use some extra hardware. Best regards, Hristo Mihalev
|
4/18/2012 11:59 AM | |
Joined: 4/16/2012 Last visit: 11/19/2012 Posts: 3 Rating:
|
Thank you all for the answers. |
4/18/2012 12:11 PM | |
Joined: 12/1/2009 Last visit: 5/2/2023 Posts: 669 Rating:
|
Dear UMENCHO, what's the advantage in using DP/DP couplers in this case?(except they cost extra money) And what stays against just using Master/Slave configuration? Regards. |
Give us your feedback and show us your respect! |
|
Follow us on